2020-12-01 4:51 PM
Is there an IOC file available for the LwIP_HTTP_Server_Netconn_RTOS Example project? I am working with the Nucleo-144 with the STM32F439ZI. Although the example project is for the 429, it works on this board. I want to be able to use CubeMX to add more middleware to the project.
Mike.
2020-12-01 11:59 PM
Dear @MStra.3 ,
You can migrate the example from one STM32 to another by following this tutorial.
Hope that this solve your issue.
Best regards,
Houssem
2020-12-02 8:38 AM
That is not what I asked for. I want an IOC file for the LwIP_HTTP_Server_Netconn_RTOS Example project so I can reconfigure the project using CubeMX.
Mike.
2025-01-03 11:33 AM
I would also like this IOC file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.