2022-11-23 6:46 AM
If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible? Can I change directory structure from cube MX or from any other tool? Like 2 applications which have different .project file, but using same STM resources like RTOS. Want to add new folders as well
2022-11-23 1:05 PM
> If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible?
Yes, entirely possible.
> Can I change directory structure from cube MX or from any other tool?
No, AFAIK the CubeMX (or the CubeIDE plugin) are not that flexible.
But one can tweak the [generated] eclipse project in various ways.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.