2020-09-25 6:12 AM
As mentioned above I can't connect as the watchdog is continuously going off. I used the STM32CubeMx to enable the IWDG and it created the s/w load which enables the IWDG but doesn't refresh it. I know how to fix it in the s/w but my debugger under TrueStudio won't connect to load the new image. My board is continuously resetting.
Have I bricked my board or is there some s/w tool I can use to erase the board? Remember I am running on linux.
Thanks in Advance for any help.
Cheers!!
Solved! Go to Solution.
2020-09-25 1:17 PM
If you enabled the IWDG hardware start, this can be disabled by using the STM32CubeProgrammer by setting some option bytes (OB).
2020-09-25 1:17 PM
If you enabled the IWDG hardware start, this can be disabled by using the STM32CubeProgrammer by setting some option bytes (OB).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.