2019-08-16 5:31 PM
OS: Ubuntu 18.04 LTS
IDE: STM32CubeIDE v1.0.1
board: STM32F769 Discovery Kit
I am trying to use LwIP with FreeRTOS.
I turned ETH, LwIP, FreeRTOS enabled in the IDE.
After generating code, I found that LwIP.c does not have MX_LWIP_Process() defined.
There is a header definition in LwIP.h, but no function declaration in LwIP.c.
Why does this happen? In this case, what should I do to use MX_LWIP_Process() in for loop.
2019-08-16 5:43 PM
I found the reason by myself.
With FreeRTOS ON, the MX_LWIP_Process() is not defined.
With FreeRTOS OFF, the MX_LWIP_Process() is defined.
2024-04-29 6:38 AM
And how to handle this issue?
I'm facing the same problem
2024-04-29 12:11 PM
MX_LWIP_Process() is only used in non-RTOS implementations. It is called from the main polling to process incoming and outgoing packets. In RTOS applications, there is a dedicated task that handles this (I don't recall the name off hand) and the MX_LWIP_Process() function is not implemented.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.