2021-01-16 6:47 AM
Hi all,
I am using a PWM timer. That is initialized and works fine.
Code for init below:
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 39;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 13;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}I start it with this call:
if (HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1) != HAL_OK) {
Error_Handler();
} if (HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1) != HAL_OK) {
Error_Handler();
}So far, so good, all works as expected. Now, I want to change the PWM pulse lenght dynamically
(I have an array of values for sConfigOC.Pulse). I found examples tha use DMA, but I really dont understand how they are working (and in my case, they dont).
So my question is: Can someone explain me in detail what needs to happen.
Questions are:
1) I can set up an DMA channel. CubeMX allows me to have TIM2_CH1 or TIM2_UP. What is the difference?
2) When I select TIM2_CH1, i can select the width of the requests on both sides. Not sure what to choose and more imporant why? The value I want to set in the register is uint32_t, so i assume, I go with word on periphal side and byte on memory side (using only values <256)?
3) How does DMA know it should copy the value in the CCR1 register? The link function that is generated by CubeMX points to the base adress of the registers.
I understand these are hard questions, but I really want to understand that inner workings, and any documentation if found left me with even more questionmarks.
Any help appreciated.
2021-01-16 3:16 PM
Which STM32?
These are hard questions mainly because you have an unnecessary extra layer between hardware and software. Cube/HAL is intended for those who wish to achieve a working program by clicking in CubeMX, which for the "usual configurations" obviously works well. Anything beyond what is deemed by Cube authors as usual means, that Cube/HAL gets into way.
I don't use Cube/HAL, I'm going to use the RM's terminology and assume, you've already read the TIM and DMA chapters in RM.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.