2023-02-15 3:36 PM
Good day sir.
ST's EVM�?development software and firmware informations or else are as below :
After modifying according to the How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working setting, currently PC PING to the EVM board�?EVM board as the TCP/UDP client that working fine. EVM board as the TCP/UDP server, after running for a while, PC can't ping the EVM board what a problem with the lwip parameter setting I guess, however that's not my point.
Currently SYS time source of test project is TIM6(1mS measurement from oscilloscope), what If I set the SYS time source to SysTick or else. are there any issues/problem problem occurred when lwip working?
2023-02-19 12:02 PM
Update your software! Before CubeH7 v1.10 the Ethernet was basically dysfunctional.
Without RTOS the SysTick is the best and default choice.
2023-02-20 1:16 AM
good day sir
Currently version of the software ,CubeMX :6.5.0, STM32Cube FW_H7 V1.10.0.
lwip 2.1.2 rawapi withour rtos.
Have any example?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.