2023-06-10 6:31 AM
Hi,
I have just installed STM32CubeIDE Version: 1.12.1 Build: 16088_20230420_1057 (UTC) onto my Kubuntu 22.04.2 LTS (fully updated) system. The install process ended stating that the IDE had been installed correctly.
I then wanted to install the package STM32Cube_FW_F4_V1.27.0. So, following the step given by community member RJepp.1 on https://community.st.com/s/question/0D53W00001vE2MNSA0/how-do-i-install-stm32cube-mcu-package-for-stm32f4-series-1271-without-an-internet-connection, I also went to (IDE) Help->Manage Embedded Software Packages. However, in my case, nothing appeared on screen. All that happened was that the Help drop down menu disappeared.
I should state that I did this while the IDE was displaying the Information Center<tab>/STM32CubeIDE Home page/screen.
In the response noted above it is stated that "1. rename the main pack from "en.stm32cubef4_v1-27-0.zip" to "stm32cube_fw_f4_v1270.zip". I did this.
The response noted above also stated that "2. Copy the zip file to the STM32CubeMx repository found under "C:\Users\the username\STM32Cube\Repository". This I also did.
Then the response states "3. Then import the patch with Help->Check for Embedded Software Packages Updates option from the local repository where you have downloaded it." This resulted in the display of a "Embedded Software Packages Manager" dialog. On the "STM32Cube MCU Packages" tab I selected first STM32F4 and then "STM32Cube Package for STM32F4 Series (Size: 657 MB) version 1.27.0" and then clicked on "From Local..."
On the resulting "Select a STM32Cube Package File" I then selected (folder) STM32Cube, then (folder) Repository, then (file) stm32cube_fw_f4_v1270.zip" and then clicked on the Open button. This resulted in the display of the "Select a STM32Cube Package File" which stated that "You cannot select a file in STM32CubeMX Repository".
Using the Dolphin FM, I checked the permissions for folders /home/username/STM32Cube and /home/username/STM32Cube/Repository. Both folders have their "rwx" permissions set for my user and group.
Folder /home/username/STM32Cube does not contain a sub-folder labelled STM32CubeMX.
What have I done wrong/left out/not understood ?
Stuart
Solved! Go to Solution.
2023-06-12 12:21 AM
First a tip: hints for the Windows version cannot necessarily be applied directly to Linux environments.
Furthermore, the firmware structure may become a little clearer if you consider the following:
Hope that helps?
Regards
/Peter
2023-06-12 12:21 AM
First a tip: hints for the Windows version cannot necessarily be applied directly to Linux environments.
Furthermore, the firmware structure may become a little clearer if you consider the following:
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.