2024-01-11 4:34 AM
Hello Team,
Hello i have a Nucleo H745ZI_Q board in this Ethernet without RTOS is working fine but when am going to configure ADC all the three ADCs are shows error message --> Partly Disabled conflict with: ETH: mode RMII even many channels also showing error message . Whats the issue ?? How to resolve this ????
Best Regards,
Gagan Gowda G R
Solved! Go to Solution.
2024-01-11 4:56 AM - edited 2024-01-12 1:53 AM
Sure, you can use everything, thats not marked as used (red).
But you cannot use pins for different functions at the same time - obviously.
This is only WARNING you, that some pins are no more available; this is no ERROR !
In your pic you see:
IN 4 , 7 , 8 no more available , = red .
IN 2 , 3 , 5 , 9 , ... still available , you can use this inputs & ethernet .
2024-01-11 4:41 AM - edited 2024-01-11 4:43 AM
>Whats the issue ??
What it tells you : some pins are not free any more, you put some function on them.
>How to resolve this ????
Set ETH to unused/disabled. Then pins are free again.
+
This is only WARNING you, that some pins are no more available; this is no ERROR !
+
You will see this yellow or red marked things more and more, when you use more peripherals.
2024-01-11 4:49 AM
2024-01-11 4:56 AM - edited 2024-01-12 1:53 AM
Sure, you can use everything, thats not marked as used (red).
But you cannot use pins for different functions at the same time - obviously.
This is only WARNING you, that some pins are no more available; this is no ERROR !
In your pic you see:
IN 4 , 7 , 8 no more available , = red .
IN 2 , 3 , 5 , 9 , ... still available , you can use this inputs & ethernet .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.