2019-07-15 12:56 AM
Hello,
I want to generate a single short pulse (adjustable between 100 ns to 1ms). What is the best way ?
I think we should use timers, but which mode ? (which CubeMX configuration ?)
Moreover I tried to configure one-pulse mode but I can't find documentation or tutorial. Either my settings (trigger mode...) are wrong, either I don't have the proper HAL command to initialise or start the pulse. Which HAL functions are needed ?
Thank you,
Valentin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.