2023-02-24 4:32 AM
Hello,
I was trying to setup a prototyping project using the NUCLEO-L031K6 examples. But the current CubeMX version 6.7.0 does not seem so know about this dev board at all.
Is this a bug or is this nucleo board not fully supported by CubeMX?
Solved! Go to Solution.
2023-02-24 6:30 AM
Hello @MKosc.1 ,
Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 6:28 AM
Welcome, @MKosc.1, to the community!
It is not a bug, the board is visible - at least on my machine. :grinning_face:
Have you installed the embedded software packages for the STM32L4?
Regards
/Peter
2023-02-24 6:30 AM
Hello @MKosc.1 ,
Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-02-24 7:01 AM
Hello,
thank you for the very fast replies! I seem to have misphrased the issue - the board is indeed visible as Peter pointed out and I can start a project based on it.
I just assumed the examples with associated .ioc files are commonly provided as well for all ST dev boards - thank you for pointing that out to me Foued.
I will proceed with the available configuration, just wanted to be sure I'm not missing something :)
2023-02-24 7:12 AM
yes sure you can share your project with me :D
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.