2018-11-20 1:42 PM
Hi,
recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:
In the log I see:
2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:919 - Problem, file not found on Server
2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:491 - Problem, file not found on Server : stm32cube_fw_f1_v170.zip.
Is v1.7.0 package available to download?
thanks,
Dmitri
2018-11-20 2:15 PM
ST looks to have got a bit ahead of themselves, issue from here also, expect it to be resolved shortly. @Khouloud GARSI
2018-11-21 2:23 AM
Hi @Dmitri ,
Issue confirmed from our side and highlighted internally.
Sorry for this inconvenience. This will be fixed ASAP!
Khouloud.
2018-11-21 3:40 AM
Hello @Dmitri
Thanks for your feedback.
FW F1 1.7.0 will be available Tomorrow after doing a refresh in update Manager.
Sorry for the inconvenience.
Best regards,
Houda
2018-11-21 6:20 AM
Hi @Dmitri ,
Issue solved: The STM32F1 v1.7.0 is now available for download.
Khouloud.
2018-11-21 9:32 AM
Confirmed, have it mirrored if anyone needs it, or the other releases. The F7.1.13.0 was 1.2GB!!
ST should really consider hosting torrents for those on lower bandwidth connections, download limits or those who have intermittent connections which might benefit from a restartable download, ie continue rather than start over...
2018-11-21 11:53 AM
Thanks for quick response!
2018-11-22 12:53 AM
You're always welcome!
2018-11-23 1:27 AM
Still having this problem. Can you provide a mirror? Thanks
2018-11-23 4:18 AM
https://drive.google.com/open?id=1-2PM2qaXjtyD7KqJ6tsvp-l0EeAPqjbo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.