STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Error downloading FW.F1.1.7.0 MCU package

Hi,recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:In the log I see:2018-11-20 23:56:39,197 [ER...

Dmitri by Associate II
  • 6242 Views
  • 12 replies
  • 0 kudos

No output on MCO1 after generating code from CubeMx

Hello,I have used CubeMx to generate a project which should do the following:configure PA8 as MCO1 and on it I want to output HSI clock which as I understand is by default 16MhzSo in CubeMx I configured PA8 as MCO1.The generated code was this:/* USER...

0690X000009YwZXQA0.png
PPopo by Senior
  • 2611 Views
  • 6 replies
  • 0 kudos

STM32CubeMX 5.3.0 doesn't work in command line mode

I'm using STM32CubeMX 5.3.0 on Linux and following the commands according to "UM1718 User manual STM32CubeMX for STM32 configuration and initialization C code generation" But the commands doesn't work and cubemx just opens directly with an error ment...

bayrem.g by Associate
  • 762 Views
  • 0 replies
  • 0 kudos

STM32F407IGTx STCubeMX strange values

Hello,I would like to know why if you are building a project with code-generated makefile for the MCU STM32F407IGTx (QFP176 pins) the linker file STM32F407ICTx_FLASH.ld tells the compiler the RAM origin at 0x20000000 has a length of 128K instead of 1...

STM32L072RB is supported by STM32CubeMX?

Hi, I need to develop a tracker with a STM32L072RBT6, I tried to generate code with STM32CubeMX v5.3.0 I'm going to use Atollic TrueStudio but Cube MX doesn't generate any code. I tries to generate a Cube MX IDE project but it's the same.is STM32L072...

Mtx_ing5 by Associate
  • 800 Views
  • 1 replies
  • 0 kudos

STM32CubeMX update to 5.3.0

The QubeMX 5.2.1 is showing update to to 5.3.0 but it fails .... also the www.st.com sometimes fails to load with direct 403 forbidden response .. some consistency will be nice :(

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.