2021-11-29 4:10 AM
The code generator is inserting the DMA_Init() and BDMA_Init functions in the wrong place, leaving DMA not working unless I manually move them after every call code generator run.
I place them in the USER CODE segment above the INIT segment then remove the auto generated versions each time otherwise DMA doesn't work.
/* USER CODE BEGIN SysInit */
MX_BDMA_Init();
MX_DMA_Init();
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_DMA_Init(); // PLACED HERE BY CODE GENERATOR
MX_LPUART1_UART_Init();
MX_BDMA_Init(); // PLACED HERE BY CODE GENERATOR
MX_I2C1_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */
Solved! Go to Solution.
2021-12-02 4:45 AM
Hi,
Thanks for the reply. This migration step fixed the issue!
Regards
matt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.