STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! DMA _Init() being called in wrong place by code generator

The code generator is inserting the DMA_Init() and BDMA_Init functions in the wrong place, leaving DMA not working unless I manually move them after every call code generator run.I place them in the USER CODE segment above the INIT segment then remov...

Resolved! USB HID device on STM32F042F4 using CubeMX - FLASH overflow.

Hi,When I set the USB class to anything in CubeMX, the compiler gives me the error - FLASH overflow. It happens even with a completely empty main.c file, so is there a way to make it work, or should I choose MCU with 32kB flash (it will fit then)? Th...

Xses by Associate II
  • 2087 Views
  • 2 replies
  • 0 kudos

ST-Link debugger connection lost after adding DMA to SPI

With STM32CubeIDE 1.7.0 (Windows) I try to setup SPI2 with DMA at an Nucleo-G431RB.After starting with an new STM32Cube C-Project for the Nucleo-G431RB with all peripherals at their default settings, I enable SPI2:Full-Duplex Master at PB[15:13]8bits...

SZwie by Associate
  • 3543 Views
  • 5 replies
  • 1 kudos

Resolved! STM32H7, Where parameter RCC.Cortex_Div is used?

I'm generating a CubeMX project for STM32H753.In the clock config, set the systick divisor 8 (see picture).Difference in the ioc file: for divisor 1:RCC.CortexFreq_Value=400000000For divisor 8:RCC.CortexFreq_Value=50000000RCC.Cortex_Div=SYSTICK_CLKS...

0693W00000GZCQZQA5.png
Pavel A. by Super User
  • 1480 Views
  • 3 replies
  • 0 kudos

STM32CubeMX 6.4.0 released

What is new in STM32CubeMX V6.4.0? • Added the support for new part numbers in the STM32L4 Series and STM32L4+ Series: STM32L443CCFx, STM32L452CETxP, STM32L452REYxP, STM32L476QGIxP, STM32L496QGIxS, STM32L4R5AIIxP, STM32L4R5QGIxS, STM32L4R5QIIxP, and ...

Resolved! HAL_CAN_INIT is producing a TIMEOUT error.

I am using CAN in normal mode and produced code using STM32CubeMX ide for Keil uVision IDE. While running the code my program stuck in HAL_CAN_INIT(). It produces a timeout error.I am not having any CAN transceiver so I am having only STM32 Nucleo Bo...

GAgar.1 by Associate
  • 1937 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX - Pinout Config - Select Alternative pins

I've been developing with STM32F4 products for years. Never used HAL or Cube products as I've hand configured everything.Beginning a new MultiCore project using STM32H745. I find using CubeMX that when I select a peripheral (like SDMMC1 or SAI4 for e...

Joe.H by Senior
  • 18032 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.