2025-12-29 4:17 AM - edited 2025-12-29 4:18 AM
It seems like CubeMX sets this default value
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;when doing software NSS and SPI Mode 3 like:
hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;This results in a non working SPI at least on STM32H652 (did not check the signals with Oscilloscope, but I assume the CLK and/or MOSI float back to an undefined value after the first transaction, breaking the next one). This can be fixed by doing:
hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;Wouldn't it be recommended CubeMX defaults the IO_STATE_ENABLE in this case?
This one Bit just cost me 5 Hours of headache :\
2025-12-29 4:30 AM
>It seems like CubeMX sets this default value
You seem to be right. :)
But no matter, Cube setting this on or off, i will always be wrong, if someone expects it just the other way.
So setting will always be "wrong" for some users.
>This one Bit just cost me 5 Hours of headache :\
Me...nothing, as i always just take a short look at all (!) settings in a peripheral, maybe there are some, i just want in a different setting. This is anyway very recommended, at least to read, what the settings are you "take" .
So i think, nothing to change or improve in Cube settings here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.