2022-05-02 9:46 PM
I've installed STM32CubeH7 library 1.10.0 manually from github.
I have CubeIDE 1.7 and CubeMX 6.3. Since they both do not understand STM32CubeH7 library version 1.10.0, I've installed CubeMX 6.5 side by side with v. 6.3.
The package manager of CubeMX 6.5 sees installed libraries v. 1.10.0 and v. 1.9.1. Fine.
But now both CubeIDE 1.7 and CubeMX 6.3 cease to see installed library v. 1.9.1, which they recognized before installation of CubeMX 6.5.
All CubeMX 6.5 and 6.3 and CubeIDE 1.7 see same installed versions of STM32CubeF0 and F4 libraries. What's the problem with H7 libraries?
OS: win11 home.
Update:
Ive removed subdirectory of v. 1.9.1. and reinstalled 1.9.0
Then all CubeMX 6.3, CubeMX 6.5, CubeIDE 1.7 see the package H7 1.9,0.
So it looks that patch H7 1.9.1 is too new for CubeMX 6.3/ CubeIDE 1.7
I don't understand why it was detected before install of CubeMX 6.5.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.