2025-04-04 4:17 AM
Hello,
create a project with the above settings and it will result in a build error (missing header file).
Thank you.
Best regards potter
Solved! Go to Solution.
2025-04-09 2:30 AM
Hello @SF49ers ,
Thank you for bringing this issue to our attention.
A ticket has been raised to the dev team in order to correct this behaviour. Internal ticket number: 207157.
Best Regards.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-04 5:33 AM
Hello @SF49ers ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest please that you provide your Ioc.File and a screenshot of the build error.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-04 6:33 AM
@SF49ers wrote:it will result in a build error (missing header file).
Is the file actually missing, or is the compiler just not finding it?
2025-04-04 1:30 PM
The CubeMX generates the source code and when you enter the folder and type "make" the generated code is missing the header file stm32g0xx.h.
- Start a project from ST Board: select NUCLEO-G031K8
- Select SYS Tab: Enable Serial Wire and set Timebase Source to TIM1
- Enable FreeRTOS CMSIS_V2
- Set a Project Name and set the Toolchain / IDE to Makefile
- Generate Code
Now open a terminal window and enter the created project folder. Type 'make' and you will get the following error message:
"... cannot open stm32g0xx.h: no such file"
If you use the FreeRTOS CMSIS_V1 instead, everything is comiling and linking fine.
Best regards potter
2025-04-09 2:30 AM
Hello @SF49ers ,
Thank you for bringing this issue to our attention.
A ticket has been raised to the dev team in order to correct this behaviour. Internal ticket number: 207157.
Best Regards.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-09 2:38 AM
That doesn't answer the question of whether the file is actually missing, or is the compiler just not finding it?
2025-04-09 9:24 AM
The answer is no and yes.
I just thought it is the better way to post a 2 minutes step by step guidance that reproduces the error, so the dev team has much less work.
2025-04-09 9:36 AM
@SF49ers wrote:The answer is no and yes.
So that tells you that the problem is in the Include Paths.
2025-07-08 12:43 AM
Hello @SF49ers
The reported problem was solved, I suggest that you try using STM32CubeMX 6.15.0, which is currently available for download through this link: STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.