2018-01-22 12:49 PM
I am currently building a project with a STM32F103RCT6 (shouldn't matter) and I ran into a problem.
CubeMX does initialize the SWD-Pins for programming. The problem seems to occur when I enable a timer peripheral on the same Port (PA8 in my case).
My workaround atm is to include a second call to '__HAL_AFIO_REMAP_SWJ_NOJTAG();' in the ' /* USER CODE BEGIN 2 */' after CubeMX is finished initializing.
I found some information in the web pointing towards this being a problem with CubeMX doing invalid read/modify/write operations on the write-only MAPR register.
I didn't find an official way to report bugs with the CubeMX tool (like github os something like that), therefore I am writing into this forum.
#stm32f103-swd-swclk-afio-mapr #cubemx-4.23 #bug?2018-03-27 6:35 AM
Hello
Dobmann.Max
,We would inform you that anew patch for STM32CubeF1 Firmware Package v1.6.1is published to fix this issue.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.