2021-05-05 5:06 AM
Hi, I try to change compiling code method to Makefile. I'm using generated from cubeMX makefile with few changes. Everything works file when I compiling main.c file but, when I change file to main.cpp compiler print errors. I tried to fix this but, my knowledge isn't enough :\
Added lines are in #VV/#^^ comments.
Now I have this error code:
....
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m3 -mthumb -DUSE_HAL_DRIVER -DSTM32L152xE -ICore/Inc -IDrivers/STM32L1xx_HAL_Driver/Inc -IDrivers/STM32L1xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32L1xx/Include -IDrivers/CMSIS/Include -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/startup_stm32l152xe.d" startup_stm32l152xe.s -o build/startup_stm32l152xe.o
arm-none-eabi-gcc -c -mcpu=cortex-m3 -mthumb -DUSE_HAL_DRIVER -DSTM32L152xE -ICore/Inc -IDrivers/STM32L1xx_HAL_Driver/Inc -IDrivers/STM32L1xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32L1xx/Include -IDrivers/CMSIS/Include -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/main.d" -Wa,-a,-ad,-alms=build/main.lst Core/Src/main.cpp -o build/main.o
arm-none-eabi-gcc build/gpio.o build/usart.o build/stm32l1xx_it.o build/stm32l1xx_hal_msp.o build/stm32l1xx_hal_tim.o build/stm32l1xx_hal_tim_ex.o build/stm32l1xx_hal_uart.o build/stm32l1xx_hal.o build/stm32l1xx_hal_rcc.o build/stm32l1xx_hal_rcc_ex.o build/stm32l1xx_hal_flash.o build/stm32l1xx_hal_flash_ex.o build/stm32l1xx_hal_flash_ramfunc.o build/stm32l1xx_hal_gpio.o build/stm32l1xx_hal_dma.o build/stm32l1xx_hal_pwr.o build/stm32l1xx_hal_pwr_ex.o build/stm32l1xx_hal_cortex.o build/stm32l1xx_hal_exti.o build/system_stm32l1xx.o build/startup_stm32l152xe.o build/main.o -mcpu=cortex-m3 -mthumb -specs=nano.specs -TSTM32L152RETx_FLASH.ld -lc -lm -lnosys -Wl,-Map=build/skytrap.map,--cref -Wl,--gc-sections -o build/skytrap.elf
c:/dev/tools/gcc-arm-none-eabi-10-2020-q4-major/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld.exe: c:/dev/tools/gcc-arm-none-eabi-10-2020-q4-major/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(lib_a-signalr.o): in function `_kill_r':
signalr.c:(.text._kill_r+0xe): undefined reference to `_kill'
c:/dev/tools/gcc-arm-none-eabi-10-2020-q4-major/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld.exe: c:/dev/tools/gcc-arm-none-eabi-10-2020-q4-major/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(lib_a-signalr.o): in function `_getpid_r':
signalr.c:(.text._getpid_r+0x0): undefined reference to `_getpid'
collect2.exe: error: ld returned 1 exit status
make: *** [build/skytrap.elf] Błąd 1Makefile:
##########################################################################################################################
# File automatically-generated by tool: [projectgenerator] version: [3.13.0-B3] date: [Wed May 05 12:06:14 GMT+02:00 2021]
##########################################################################################################################
# ------------------------------------------------
# Generic Makefile (based on gcc)
#
# ChangeLog :
# 2017-02-10 - Several enhancements + project update mode
# 2015-07-22 - first version
# ------------------------------------------------
######################################
# target
######################################
TARGET = skytrap
######################################
# building variables
######################################
# debug build?
DEBUG = 1
# optimization
OPT = -Og
#######################################
# paths
#######################################
# Build path
BUILD_DIR = build
######################################
# source
######################################
# C sources
#VV there remove main.c
C_SOURCES = \
Core/Src/gpio.c \
Core/Src/usart.c \
Core/Src/stm32l1xx_it.c \
Core/Src/stm32l1xx_hal_msp.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_tim.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_tim_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_uart.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_rcc.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_rcc_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ramfunc.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_gpio.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_dma.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_pwr.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_pwr_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_cortex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_exti.c \
Core/Src/system_stm32l1xx.c
# ASM sources
ASM_SOURCES = \
startup_stm32l152xe.s
#VV
CXXSRC= \
Core/Src/main.cpp
#^^
#######################################
# binaries
#######################################
PREFIX = arm-none-eabi-
# The gcc compiler bin path can be either defined in make command via GCC_PATH variable (> make GCC_PATH=***)
# either it can be added to the PATH environment variable.
ifdef GCC_PATH
CC = $(GCC_PATH)/$(PREFIX)gcc
AS = $(GCC_PATH)/$(PREFIX)gcc -x assembler-with-cpp
CP = $(GCC_PATH)/$(PREFIX)objcopy
SZ = $(GCC_PATH)/$(PREFIX)size
else
CC = $(PREFIX)gcc
AS = $(PREFIX)gcc -x assembler-with-cpp
CP = $(PREFIX)objcopy
SZ = $(PREFIX)size
endif
HEX = $(CP) -O ihex
BIN = $(CP) -O binary -S
#######################################
# CFLAGS
#######################################
# cpu
CPU = -mcpu=cortex-m3
# fpu
# NONE for Cortex-M0/M0+/M3
# float-abi
# mcu
MCU = $(CPU) -mthumb $(FPU) $(FLOAT-ABI)
# macros for gcc
# AS defines
AS_DEFS =
# C defines
C_DEFS = \
-DUSE_HAL_DRIVER \
-DSTM32L152xE
# AS includes
AS_INCLUDES =
# C includes
C_INCLUDES = \
-ICore/Inc \
-IDrivers/STM32L1xx_HAL_Driver/Inc \
-IDrivers/STM32L1xx_HAL_Driver/Inc/Legacy \
-IDrivers/CMSIS/Device/ST/STM32L1xx/Include \
-IDrivers/CMSIS/Include
# compile gcc flags
ASFLAGS = $(MCU) $(AS_DEFS) $(AS_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections
CFLAGS = $(MCU) $(C_DEFS) $(C_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections
ifeq ($(DEBUG), 1)
CFLAGS += -g -gdwarf-2
endif
# Generate dependency information
CFLAGS += -MMD -MP -MF"$(@:%.o=%.d)"
#######################################
# LDFLAGS
#######################################
# link script
LDSCRIPT = STM32L152RETx_FLASH.ld
# libraries
LIBS = -lc -lm -lnosys
LIBDIR =
LDFLAGS = $(MCU) -specs=nano.specs -T$(LDSCRIPT) $(LIBDIR) $(LIBS) -Wl,-Map=$(BUILD_DIR)/$(TARGET).map,--cref -Wl,--gc-sections
# default action: build all
all: $(BUILD_DIR)/$(TARGET).elf $(BUILD_DIR)/$(TARGET).hex $(BUILD_DIR)/$(TARGET).bin
#######################################
# build the application
#######################################
# list of objects
OBJECTS = $(addprefix $(BUILD_DIR)/,$(notdir $(C_SOURCES:.c=.o)))
vpath %.c $(sort $(dir $(C_SOURCES)))
# list of ASM program objects
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(ASM_SOURCES:.s=.o)))
vpath %.s $(sort $(dir $(ASM_SOURCES)))
#VV
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(CXXSRC:.cpp=.o)))
vpath %.cpp $(sort $(dir $(CXXSRC)))
#^^
$(BUILD_DIR)/%.o: %.c Makefile | $(BUILD_DIR)
$(CC) -c $(CFLAGS) -Wa,-a,-ad,-alms=$(BUILD_DIR)/$(notdir $(I hope someone can resolve this issue =)
I will be grateful for any help.
@Edit:
I'm not sure if I need to use G++ compiler for .cpp files?
GCC ver: gcc-arm-none-eabi-10-2020-q4-major
openocd ver: openocd-20210503
2021-05-05 7:38 AM
> I'm not sure if I need to use G++ compiler for .cpp files?
Yes, of course you do. G++ for C++ and gcc for C.
2021-05-05 2:50 PM
You need to add the g++ compiler:
PREFIX = arm-none-eabi-
ifdef GCC_PATH
CC = $(GCC_PATH)/$(PREFIX)gcc
CPP = $(GCC_PATH)/$(PREFIX)g++
AS = $(GCC_PATH)/$(PREFIX)gcc -x assembler-with-cpp
CP = $(GCC_PATH)/$(PREFIX)objcopy
SZ = $(GCC_PATH)/$(PREFIX)size
else
CC = $(PREFIX)gcc
CPP = $(PREFIX)g++
AS = $(PREFIX)gcc -x assembler-with-cpp
CP = $(PREFIX)objcopy
SZ = $(PREFIX)size
endif
Also you need to add sources, includes, and cppflags:
CPP_SOURCES = \
Core/Src/main.cpp \
CPP_INCLUDES = \
Core/Inc \
CPPFLAGS = $(CPP_INCLUDES) -std=c++17 -Wno-register
And add this in the build application section:
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(CPP_SOURCES:.cpp=.o)))
vpath %.cpp $(sort $(dir $(CPP_SOURCES)))
$(BUILD_DIR)/%.o: %.cpp Makefile | $(BUILD_DIR)
$(CPP) -c $(CFLAGS) $(CPPFLAGS) -Wa,-a,-ad,-alms=$(BUILD_DIR)/$(notdir $(<:.cpp=.lst)) $< -o $@
2021-05-06 7:13 AM
I did few updates, but still do not work and have the same error. For example, I changed the CXXFLAGS. When I change CXXF. on "#CXXFLAGS = $(C_INCLUDES) -std=c++17 -Wno-register #ERROR 1" I had an error like below [ERROR 1]
...................
139 | RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
| ^~~~~~~~~~~~~~~
Core/Src/main.cpp:140:21: error: 'struct RCC_ClkInitTypeDef' has no member named 'APB1CLKDivider'
140 | RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
| ^~~~~~~~~~~~~~
In file included from Core/Inc/stm32l1xx_hal_conf.h:197,
from Drivers/STM32L1xx_HAL_Driver/Inc/stm32l1xx_hal.h:30,
from Core/Inc/main.h:31,
from Core/Src/main.cpp:21:
Drivers/STM32L1xx_HAL_Driver/Inc/stm32l1xx_hal_rcc.h:477:42: error: 'RCC_CFGR_PPRE1_DIV1' was not declared in this scope
477 | #define RCC_HCLK_DIV1 RCC_CFGR_PPRE1_DIV1 /*!< HCLK not divided */
| ^~~~~~~~~~~~~~~~~~~
Core/Src/main.cpp:140:38: note: in expansion of macro 'RCC_HCLK_DIV1'
140 | RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
| ^~~~~~~~~~~~~
Core/Src/main.cpp:141:21: error: 'struct RCC_ClkInitTypeDef' has no member named 'APB2CLKDivider'
141 | RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
| ^~~~~~~~~~~~~~
In file included from Core/Inc/stm32l1xx_hal_conf.h:233,
from Drivers/STM32L1xx_HAL_Driver/Inc/stm32l1xx_hal.h:30,
from Core/Inc/main.h:31,
from Core/Src/main.cpp:21:
Drivers/STM32L1xx_HAL_Driver/Inc/stm32l1xx_hal_flash.h:144:36: error: 'FLASH_ACR_LATENCY' was not declared in this scope; did you mean 'FLASH_LATENCY_1'?
144 | #define FLASH_LATENCY_1 FLASH_ACR_LATENCY /*!< FLASH One Latency cycle */
| ^~~~~~~~~~~~~~~~~
Core/Src/main.cpp:143:47: note: in expansion of macro 'FLASH_LATENCY_1'
143 | if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
| ^~~~~~~~~~~~~~~
Core/Src/main.cpp: In function 'void Error_Handler()':
Core/Src/main.cpp:161:3: error: '__disable_irq' was not declared in this scope
161 | __disable_irq();
| ^~~~~~~~~~~~~
make: *** [build/main.o] Błąd 1Also updated makefile
##########################################################################################################################
# File automatically-generated by tool: [projectgenerator] version: [3.13.0-B3] date: [Wed May 05 12:06:14 GMT+02:00 2021]
##########################################################################################################################
# ------------------------------------------------
# Generic Makefile (based on gcc)
#
# ChangeLog :
# 2017-02-10 - Several enhancements + project update mode
# 2015-07-22 - first version
# ------------------------------------------------
######################################
# target
######################################
TARGET = skytrap
######################################
# building variables
######################################
# debug build?
DEBUG = 1
# optimization
OPT = -Og
#######################################
# paths
#######################################
# Build path
BUILD_DIR = build
######################################
# source
######################################
# C sources
#VV there remove main.c
C_SOURCES = \
Core/Src/gpio.c \
Core/Src/usart.c \
Core/Src/stm32l1xx_it.c \
Core/Src/stm32l1xx_hal_msp.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_tim.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_tim_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_uart.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_rcc.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_rcc_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_flash_ramfunc.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_gpio.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_dma.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_pwr.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_pwr_ex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_cortex.c \
Drivers/STM32L1xx_HAL_Driver/Src/stm32l1xx_hal_exti.c \
Core/Src/system_stm32l1xx.c
# ASM sources
ASM_SOURCES = \
startup_stm32l152xe.s
#VV
CXX_SOURCES= \
Core/Src/main.cpp
#^^
#######################################
# binaries
#######################################
PREFIX = arm-none-eabi-
# The gcc compiler bin path can be either defined in make command via GCC_PATH variable (> make GCC_PATH=***)
# either it can be added to the PATH environment variable.
ifdef GCC_PATH
CC = $(GCC_PATH)/$(PREFIX)gcc
#VV
CXX = $(GCC_PATH)/$(PREFIX)g++
#^^
AS = $(GCC_PATH)/$(PREFIX)gcc -x assembler-with-cpp
CP = $(GCC_PATH)/$(PREFIX)objcopy
SZ = $(GCC_PATH)/$(PREFIX)size
else
CC = $(PREFIX)gcc
#VV
CXX = $(PREFIX)g++
#^^
AS = $(PREFIX)gcc -x assembler-with-cpp
CP = $(PREFIX)objcopy
SZ = $(PREFIX)size
endif
HEX = $(CP) -O ihex
BIN = $(CP) -O binary -S
#######################################
# CFLAGS
#######################################
# cpu
CPU = -mcpu=cortex-m3
# fpu
# NONE for Cortex-M0/M0+/M3
# float-abi
# mcu
MCU = $(CPU) -mthumb $(FPU) $(FLOAT-ABI)
# macros for gcc
# AS defines
AS_DEFS =
# C defines
C_DEFS = \
-DUSE_HAL_DRIVER \
-DSTM32L152xE
# AS includes
AS_INCLUDES =
# C includes
C_INCLUDES = \
-ICore/Inc \
-IDrivers/STM32L1xx_HAL_Driver/Inc \
-IDrivers/STM32L1xx_HAL_Driver/Inc/Legacy \
-IDrivers/CMSIS/Device/ST/STM32L1xx/Include \
-IDrivers/CMSIS/Include
CXX_INCLUDES = \
-ICore/Inc
# compile gcc flags
ASFLAGS = $(MCU) $(AS_DEFS) $(AS_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections
CFLAGS = $(MCU) $(C_DEFS) $(C_INCLUDES) $(OPT) -Wall -fdata-sections -ffunction-sections -std=c99
#CXXFLAGS = $(MCU) $(C_DEFS) $(C_INCLUDES) $(OPT) -std=c++17 -Wno-register #ERROR 0
CXXFLAGS = $(C_INCLUDES) -std=c++17 -Wno-register #ERROR 1
ifeq ($(DEBUG), 1)
CFLAGS += -g -gdwarf-2
endif
# Generate dependency information
CFLAGS += -MMD -MP -MF"$(@:%.o=%.d)"
#######################################
# LDFLAGS
#######################################
# link script
LDSCRIPT = STM32L152RETx_FLASH.ld
# libraries
LIBS = -lc -lm -lnosys
LIBDIR =
LDFLAGS = $(MCU) -specs=nano.specs -T$(LDSCRIPT) $(LIBDIR) $(LIBS) -Wl,-Map=$(BUILD_DIR)/$(TARGET).map,--cref -Wl,--gc-sections
# default action: build all
all: $(BUILD_DIR)/$(TARGET).elf $(BUILD_DIR)/$(TARGET).hex $(BUILD_DIR)/$(TARGET).bin
#######################################
# build the application
#######################################
# list of objects
OBJECTS = $(addprefix $(BUILD_DIR)/,$(notdir $(C_SOURCES:.c=.o)))
vpath %.c $(sort $(dir $(C_SOURCES)))
# list of ASM program objects
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(ASM_SOURCES:.s=.o)))
vpath %.s $(sort $(dir $(ASM_SOURCES)))
#VV
OBJECTS += $(addprefix $(BUILD_DIR)/,$(notdir $(CXX_SOURCES:.cpp=.o)))
vpath %.cpp $(sort $(dir $(CXX_SOURCES)))
#^^
$(BUILD_DIR)/%.o: %.c Makefile | $(BUILD_DIR)
$(CC) -c $(CFLAGS) -Wa,-a,-ad,-alms=$(BUILD_DIR)/$(notdir $(
2021-05-06 2:21 PM
Hi,
I m not sure about your errors!!
But i think it could be including c files in a cpp project. To use c files in a cpp file. Make sure that the C headers are inside extern "C" { ... } block.
So the C files you include in a cpp project need to be inside a extern "C" { ... } block.
So for example if you include main.h in main.cpp, the code from main.h need to be inside this block.
Example main.h
#ifndef __MAIN_H
#define __MAIN_H
#ifdef __cplusplus
#ifdef __cplusplus
extern "C" {
#endif
//main contents of header
//here goes the code from main.h
#ifdef __cplusplus
}
#endif
#endif /* MAIN_H*/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.