cancel
Showing results for 
Search instead for 
Did you mean: 

cubemx + errata

yakabmarci
Senior
Posted on June 08, 2016 at 18:10

I would propose to update the cubemx sw to consider also the errata/chip bugs, to implement the workaround (where there is one) or mark setting as invalid.

The tool itself(cubemx) is a very good idea in general, it would save some hours of configuration if it worked. The problem is that it doesn't always work , and you don't know why, then spend hours verifying each bit, then the errata, only to see that the generated configuraiton is not valid, so at the end you have wasted some hours instead of saving any.

I had problems with SPI and I2C configurations (both were errata items, btw the I2C is pretty messed up, the amount of bugs/limitations are comparable with the amount of features)

The chip in question was stm32f100rb cube fw and mx, the latest to this date.

#cubemx-errata-bug
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stm32cube-t
ST Employee
Posted on June 10, 2016 at 13:36

Dear user,

Point taken.

Sorry for the inconvenience.

stm32cube-t
ST Employee
Posted on October 06, 2016 at 17:18

Dear user,

Please check STM32CubeMX release 4.16 that implements errata sheet.

Best regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.