2024-01-26 3:22 AM
在使用CubeMX生成Makefile工程文件时,在Mid中间件选项中选择“X-CUBE_ALGOBUILD”选项,并添加DSP Library,但是在最后的生成的项目文件中并没哟dsp.lib文件,应该是一个bug,望修复
2024-01-26 6:23 AM
> When using CubeMX to generate the Makefile project file, select the "X-CUBE_ALGOBUILD" option in the Mid middleware option and add the DSP Library. However, there is no dsp.lib file in the final generated project file. This should be a bug. hope to repair
2024-01-26 6:33 AM
Yes,this is what i mean
2024-01-29 1:10 AM
Hello,
First let me thank you for posting.
Can you provide please the STM32CubeMx version.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-29 2:14 AM
6.9.1
2024-01-30 12:14 AM
2024-01-30 2:33 AM
应该是我的中文路径影响到了,同时我也没找到那天我创建的文件夹,今天我又试了试,可以了
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.