2018-02-03 11:16 PM
Hello!
I found a problem with initialization code generated for TIM2 when you select Clock source as ETR2. The bug is with pin initialization for alternate function: GPIO_InitStruct.Alternate is not set to any value (let alone the desired one):
Inside function HAL_TIM_Base_MspInit:
/**TIM2 GPIO Configuration
PA0-WKUP ------> TIM2_ETR
*/
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
The version of CubeMX is 4.0
The problem is only with TIM2, all other timers generate proper code.
Regards,
Maciej
#cubemx-bug #cubemx-bug-report2018-02-12 1:13 AM
Hello
xt1
,I have just tried with CubeMX4.24 and MCU STM32L476VGTx (with TIM2 and ETR2 set as clock source). Here is the code generated :
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{......
PA0 ------> TIM2_ETR */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF14_TIM2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* USER CODE BEGIN TIM2_MspInit 1 */
==> Issue is not present.
Could you please tell me what MCU you are using? (the best would be to send me your ioc in order that I understand the issue).
Thanks in advance.
Jeanne
2018-02-12 3:45 AM
Hi
,The MCU is stm32F207, see the attached project file.
Regards
Maciej Musiał
________________ Attachments : bug.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy0Q&d=%2Fa%2F0X0000000b36%2FtG1Ya.aAkX80d_zJPUYpwXNiWvmLiOVV_kzsZ52HRaw&asPdf=false2018-02-12 6:28 AM
hello
xt1
,Thanks for your ioc, I see your point.
I will keep you inform as soon as there is a change on that point.
Sorry for the inconvenience it may cause.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.