2025-09-29 1:26 AM - last edited on 2025-09-29 1:55 AM by Andrew Neil
For the STM32H743IIKx micro, CubeMX 6.15.0 unnecessarily creates a configuration for the R1 pin when creating an LTDC peripheral when using the RGB666 Display Type.
This should not be configured. The required R* pins for this Display Type are R2-R7, as per G2-G7 and B2-B7.
This did not occur in previous CubeMX versions, including 6.14.1.
This bug means that it is not possible to upgrade to this version of CubeMX with an existing project that already uses the pin(s) required for LTDC_R1.
Solved! Go to Solution.
2025-09-29 2:25 AM
Hello @Craig_Robertson ,
It is a regression on the STM32CubeMX V6.15.0.
This is a known Issue, and an internal Ticket was submitted to the Development Team
(Internal Ticket Number: 215387).
I will keep you up to date when the problem is solved.
Best Regards.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-29 1:52 AM
Hello @Craig_Robertson ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-29 2:25 AM
Hello @Craig_Robertson ,
It is a regression on the STM32CubeMX V6.15.0.
This is a known Issue, and an internal Ticket was submitted to the Development Team
(Internal Ticket Number: 215387).
I will keep you up to date when the problem is solved.
Best Regards.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-29 4:57 PM
Thanks very much for the quick reply.
2025-10-22 1:48 AM - edited 2025-10-22 1:53 AM
Hello,
Any news on this ?
The fix I am using now is to modify the generated source code. This is not satisfying.
Note that when migrating a project to 6.15.0, LTDC configuration is removed without user notification because there is no pin available for LTDC_R1.
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.