2025-07-16 4:58 AM - last edited on 2025-07-17 6:19 AM by Amel NASRI
hi,
cube ide updated with latest version 1.19.0 have bug as below picture .
By default quad spi is disabled and i could able to select quad spi in older version cube mx by using old project and continue with old cube mx version not migrate .
Solved! Go to Solution.
2025-07-16 5:58 AM
Hello @MMARI.1 ,
The same issue was reported on these posts:
STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (ST... - STMicroelectronics Community
STM32CUBEIDE Version: 1.19.0 QUADSPI unavailable ... - STMicroelectronics Community
An Internal Ticket was raised to the Development Team ( Ticket Number: 213718 ).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-16 5:01 AM
you haven't said what chip you're using!
2025-07-16 5:03 AM
hi neil,
stm32h723zgt6 with w25q128
2025-07-16 5:58 AM
Hello @MMARI.1 ,
The same issue was reported on these posts:
STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (ST... - STMicroelectronics Community
STM32CUBEIDE Version: 1.19.0 QUADSPI unavailable ... - STMicroelectronics Community
An Internal Ticket was raised to the Development Team ( Ticket Number: 213718 ).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-18 8:42 AM
Hello Mahmoud
I have the same issue after upgrading to V1.19. My quad SPI port became disabled and I cannot enable QSPI for either port. I am using STM32H7A3 processor. When I hover over QSPI for port 1, it says QSPI2 is already active. When I hover over QSPI for port 2, it says QSPI1 is already active. However, both are disabled.
Thanks,
Dan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.