2025-03-11 2:10 AM
Hello,
In CubeIDE I try to generate RTC code which has decimal parameters. However in code generation I realized that it converted to hex value by itself.
You can check screen shots in the attachment.
2025-03-11 2:40 AM
Hello @farukisiker
Thank you for posting!
Could you mention the name of the MCU where you encountered the issue?
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-11 2:45 AM - edited 2025-03-11 2:46 AM
This behavior is correct. 12 decimal expressed in BCD format is 0x12. If you change it to binary format, it will be 12.
2025-03-11 3:26 AM
Stm32H7 Series
2025-03-11 3:33 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.