cancel
Showing results for 
Search instead for 
Did you mean: 

CubeIDE 1.3.0 for STM32L4R5 MCUPackage 1.15.1 creates faulty LPUART1 IRQ Handler

Johannes
Senior

I use CubeIDE 1.3.0 and STM32L4 MCU Package 1.15.1.

I wanted to setup a demo project for Nucleo-L4R5ZI.

these boards route LPUART1 to STLINK debug Uart port.

If you enable NVIC for LPUART1, the firmware package creates a faulty IRQ handler. It should pass HLPUART1 to the IRQ handler but it passes HUART1 (which is not used and not initialized)

void LPUART1_IRQHandler(void)
{
  /* USER CODE BEGIN LPUART1_IRQn 0 */
 
	/* USER CODE END LPUART1_IRQn 0 */
  HAL_UART_IRQHandler(&huart1);
  /* USER CODE BEGIN LPUART1_IRQn 1 */
 
  /* USER CODE END LPUART1_IRQn 1 */
}

Workaround:

void LPUART1_IRQHandler(void)
{
  /* USER CODE BEGIN LPUART1_IRQn 0 */
  HAL_UART_IRQHandler(&lphuart1);
  return;
 
	/* USER CODE END LPUART1_IRQn 0 */
  HAL_UART_IRQHandler(&huart1);
  /* USER CODE BEGIN LPUART1_IRQn 1 */
 
  /* USER CODE END LPUART1_IRQn 1 */
}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @jvisser,

Good news :) I am pleased to inform you that this issue is fixed in the latest STM32CubeMX version 6.2.0.

The LPUART1 IRQ Handler is correctly generated by CubeMX.

Thank you for your contribution.

Khouloud.

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee

Hi @Johannes​ ,

Thanks for bringing this issue to our attention. It is reported to our STM32CubeMX development team.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @jvisser,

Good news :) I am pleased to inform you that this issue is fixed in the latest STM32CubeMX version 6.2.0.

The LPUART1 IRQ Handler is correctly generated by CubeMX.

Thank you for your contribution.

Khouloud.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.