2024-04-26 7:54 AM
Hello,
I use STM32CubeMX V6.11.1 with cmake version 3.28.1 (the one embedded in STM32CubeCLT_1.15.1) to generate a project for STM32F746G Discovery kit.
When trying the new cmake project generation feature in conjunction with CubeAI, the generated project is not building.
I get the error:
Solved! Go to Solution.
2025-02-08 7:05 AM
Hello @jjaccard
I’m not able to reproduce this behavior with the STM32CubeMX V6.13.0. If you still have the same issue, please tel me to check this again for you @Remyhx , please create a new post on the wireless forum since it is a wireless product related your issue with a description of all your case details and with a .ioc file that reproduce your behavior on the CubeMX V6.13.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-26 12:35 PM
Hello @jjaccard and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Can you share your .ioc file so we can try to reproduce (with a description on how you did it if possible).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-29 1:55 AM
Hello,
Thanks for the welcome : )
Sure, you can find linked the .ioc file. As mentionned above, I created a project with STM32CubeMX V6.11.1 for STM32F746G Discovery kit (all default periph.). I then added X-CUBE-AI V9.0.0 with the application template and added a simple dense .tflite model. Finally I generated the code for cmake toolchain.
Then I followed your video to open and import the cmake project in vscode: https://www.youtube.com/watch?v=DDVdq47Dd94
And when I try to build, the issue mentioned in my original post arise. As mentioned above, I can fix it but every time I want to change something in CubeMx and regenerate the code I have to re-fix the build system (when I update the .tflite model for example, which happens quite often).
Thanks in advance for the help.
Jérémie
2024-06-03 8:48 AM
Hello,
Any news on this issue?
Thanks
2025-02-08 6:54 AM
Same kind of mistake here: STM32WB with first ble included, later excluded. Had to remove tinylpm.c from cmake/stm32cubemx/cmakelists.txt. Every time I regenerate the project it has to manually be removed.
I see no follow up from STM.
2025-02-08 7:05 AM
Hello @jjaccard
I’m not able to reproduce this behavior with the STM32CubeMX V6.13.0. If you still have the same issue, please tel me to check this again for you @Remyhx , please create a new post on the wireless forum since it is a wireless product related your issue with a description of all your case details and with a .ioc file that reproduce your behavior on the CubeMX V6.13.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-10 9:19 AM
Also 6.13.0, migrated from 6.12. Couple of times gave me the error, but somehow it vanished. Thx for the reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.