2020-08-06 6:23 AM
Hello!
Before I forget:
I'm using Windows 10. Fresh machine.
I have downloaded the latest CubeMX. When I wanted to install it, it asked me for Java, so I installed the latest Java. Now it says:
The application requires a Java Runtime Environment 1.8.0_45 (64 bit). But the only one I could find is the one which is downloadable now, which is newer than _045. Actually the version is 1.8.0_261. Does anyone have a solution to this problem?
Thanks,
Pascal
2020-08-06 6:43 AM
Perhaps search for "jre-8u251-windows-x64.exe". But pay attention on the licensing terms of Oracle.
2020-08-06 7:27 AM
Hello!
Thanks for your reply!
In the meantime, I did it to be sure that a x64 version is installed. For those who may get the same problem,
I downloaded the offline version, x64, and again, I'm working with Windows.
> But pay attention on the licensing terms of Oracle.
What do you mean? Are the terms different to the version which is downloaded automatically? I have absolutely
no knowledge about legal matters, I just assume that java realtime environment is free.
Now this solved my problem concerning (re)installation of CubeMX, but not the ground problem.
Here it is:
but after that nothing worked.
same, stuck in code generation's "copying libraries". The good news is that I could fix my main PC's Cube install
problem, but that's about it, Cube doesn't work yet.
Any hint?
Thnaks,
Pascal
2020-11-14 2:03 AM
The magic sauce here is to install 64 bit java, It appears the default (e.g. Minecraft) is 32 bit.
,,,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.