2020-09-21 11:36 PM
Hi
After updating to CubeMx 6.0.1 and my STM32H7 Pack to 1.8.0 I cannot create project code for Keil uVision 5.27.
After pushing the create code button it brings up the progress bar, seems to be doing stuff and then brings up a dialog:
---------------------------------------------------------------------------------------------------------------------------------------
"The code is successfully generated under G:/LoranReceiver_002 but MDK-ARM V5.27 project generation have problem."
---------------------------------------------------------------------------------------------------------------------------------------
When I open uVision I get an error:
--------------------------------------------------------------
"Error: Device not found -
Device: '??device??'
Vendor 'STMicroelectronics'
Please update your device selection."
--------------------------------------------------------------
The uVision file tree is empty of files and when you open the uVision config dialog no device is selected.
I tried the same project with Atollic and it worked fine.
I have not made any changes to uVision 5 since I used it successfully with older versions of CubeMX.
All my MCU packages are up to date in uVision.
I tried ti with an STM32H743ZIT and an STM32F411RE and had the same problem with each.
I have NEVER had any problems with the CubeMX uVision 5.xx before today.
An no I'm not going to change to TrueStudio, it's hard way of doing a simple job and I don't want to waste my time grappling with Eclipse.
Can anybody assist?
Best regards
Rob
2020-10-06 8:55 PM
2020-10-06 9:27 PM
2020-10-13 1:06 AM
Hello,
I have had the same problem.
The solution was to reinstall the java environment.
Regards
Horst
2020-10-20 8:32 PM
2020-10-21 10:53 AM
Hello Rob,
I have had the same problem.
The solution was to reinstall the java environment.
Regards
Horst
2020-10-21 4:26 PM
Hi Horst,
Thanks for that, but could you elaborate. I have a 64 bit computer an Windows system.
I have a few different java versions on my machine as I use Anywhere Softwares B4J which uses two different versions of java depending on whether you are creating a UI or headless app.
Best regards
Rob
2020-10-21 11:33 PM
I have this problem. I installed all version of java. but it does not work yet
2020-10-22 11:37 AM
Hello Rob,
I have Windows10-64Bit on my computer.
Here are the steps that I did:
Thats all.
The installation process of CubeMX under step 3 is asking for the installation of Java. When you accept this, then the newest Java version is installed under the path C:\Program Files (x86)\Java\..... This did not work on my computer!!! I suppose CubeMX does have a problem with Java in the path "Program Files (x86)".
Kind regards
Horst
2020-10-22 9:05 PM
2020-10-22 9:17 PM
Hi Horst,
Thanks for that I will give it a try.
Best regards
Rob
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.