2023-08-10 6:32 AM
2023-08-17 1:27 AM
Hello @Kamil Duljas
First let me thank you for posting.
I assume this is the exact same request CubeMX feature request: Is it possible to add HAL_... - STMicroelectronics Community already raised to the development team and tracked by the Tickets 148949 and 149021 and that will be added to CubeMX as soon as possible.
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-11 1:30 AM
Hello @Kamil Duljas ,
which filters do you want to use ?
Could you please share more information ?
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-14 12:21 AM
I just communicate 2 stm32F7 boards through CAN and I see in examples need to configure
CAN_FilterTypeDef CAN_FilterInitStructure
but I don't see any settings in CubeMX
2023-08-14 2:14 AM
Hello @Kamil Duljas ,
You need too add can filters into the code, for example :
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
I suggest you check the available example in the stm32f7 cubefw : STM32Cube_FW_F7_V1.17.0\Projects\STM32756G_EVAL\Examples\CAN
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-14 2:50 AM
Ok, but why i can't set this settings via CubeMx?
2023-08-17 1:27 AM
Hello @Kamil Duljas
First let me thank you for posting.
I assume this is the exact same request CubeMX feature request: Is it possible to add HAL_... - STMicroelectronics Community already raised to the development team and tracked by the Tickets 148949 and 149021 and that will be added to CubeMX as soon as possible.
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.