2026-01-29 4:40 AM
From cube 1.3.0 I always get this error and the cause seems to be the path generation in .d files. In cube 1.12.1 the path is relative but from cube 1.3.0 it is absolute and generates something like \\?\C:\.... So the only solution for me is to stay with cube 1.12.0. The build however seems ok an the bin file is generated. Did anyone had a similar issue? The issue is present only on windows and it seems ok on linux.
arm-none-eabi-size STM32F769I_TEST.elf
arm-none-eabi-objdump -h -S STM32F769I_TEST.elf > "STM32F769I_TEST.list"
arm-none-eabi-objcopy -O ihex STM32F769I_TEST.elf "STM32F769I_TEST.hex"
arm-none-eabi-objcopy -O binary STM32F769I_TEST.elf "STM32F769I_TEST.bin"
text data bss dec hex filename
1227608 43680 452264 1723552 1a4ca0 STM32F769I_TEST.elf
Finished building: default.size.stdout
Finished building: STM32F769I_TEST.hex
Finished building: STM32F769I_TEST.bin
Finished building: STM32F769I_TEST.list
test/web/unicabminnow.d:1: *** multiple target patterns. Stop.
make: *** [makefile:152: all] Error 2
"make -j8 all" terminated with exit code 2. Build might be incomplete.
12:23:07 Build Failed. 3 errors, 408 warnings. (took 1m:27s.726ms)
2026-01-29 5:11 AM
Hello @aljo666
Let me thank you for posting.
I recommend that you use the last version STM32CubeIDE 2.0.
STM32CubeIDE | Software - STMicroelectronics
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-29 5:13 AM
Already tired and the issue is still present.
2026-01-29 5:21 AM
Could you provide please your STM32CubeIDE Project.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-29 6:40 AM
I cannot provide you the project but here is the difference in the .d file for long paths. The main project has links to a basic project and you can see that cube 2.0 generates absolute path and cube 1.2 generates relative paths in .d files which I think throws the error.
stm32 cubeide 2.0.0.0
\\?\C:\Projects\274_Ship_smart_cabin\UNIcabSVN\UNIcab\STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I-Discovery\Applications\Datapan\UNIcab\Src\Datapan\FreeRTOS-Plus\FreeRTOS-IoT-Libraries\abstractions\platform\freertos\include\platform\iot_platform_types_freertos.h \ Datapan/UNIcabWeb/unicabminnow.d:1: *** multiple target patterns. Stop.
stm32 cubeide 1.12.1 ../../../../../../../274_Ship_smart_cabin/UNIcabSVN/UNIcab/STM32Cube_FW_F7_V1.15.0/Projects/STM32F769I-Discovery/Applications/Datapan/UNIcab/Src/Datapan/FreeRTOS-Plus/FreeRTOS-IoT-Libraries/abstractions/platform/freertos/include/platform/iot_platform_types_freertos.h \ build ok
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.