2019-07-18 12:04 AM
hello,
i generated the code using CubeMX and the last version of F7-Package(V1.15.0) and i noticed that the generated code used the wrong pins for RMII.
the wrong generated code used:
PB11 ------> ETH_TX_EN
PB12 ------> ETH_TXD0
the right one should be:
PG11 ------> ETH_TX_EN
PG13 ------> ETH_TXD0
this should be modified in two functions:
void HAL_ETH_MspInit(ETH_HandleTypeDef* ethHandle)
void HAL_ETH_MspDeInit(ETH_HandleTypeDef* ethHandle)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.