2019-10-19 5:26 AM
Hello,
I think the correct range for TCPIP_THREAD_PRIO, DEFAULT_THREAD_PRIO, SLIPIF_THREAD_PRIO and possible others in CubeMX LWIP configuration should be -3 to +3 and not 0 to 6.
And the default value should be lower than 3 (osPriorityRealtime) definitely to avoid conflicts with low level ETH send/receive threads.
2020-01-09 6:36 AM
Ok, the issue seems to been fixed since new CubeMX 5.5.0, at least for TCPIP_THREAD_PRIO in generated file lwipopts.h
/*----- Value in opt.h for TCPIP_THREAD_PRIO: 1 -----*/
#define TCPIP_THREAD_PRIO osPriorityNormal
/*----- Value in opt.h for SLIPIF_THREAD_PRIO: 1 -----*/
#define SLIPIF_THREAD_PRIO 3
/*----- Value in opt.h for DEFAULT_THREAD_PRIO: 1 -----*/
#define DEFAULT_THREAD_PRIO 3Now a value of 3 in CubeMX is interpreted as osPriorityNormal (0) correctly
typedef enum {
osPriorityIdle = -3, ///< priority: idle (lowest)
osPriorityLow = -2, ///< priority: low
osPriorityBelowNormal = -1, ///< priority: below normal
osPriorityNormal = 0, ///< priority: normal (default)
osPriorityAboveNormal = +1, ///< priority: above normal
osPriorityHigh = +2, ///< priority: high
osPriorityRealtime = +3, ///< priority: realtime (highest)
osPriorityError = 0x84 ///< system cannot determine priority or thread has illegal priority
} osPriority;Could you check if the same issue also matches the interpretation for SLIPIF_THREAD_PRIO and DEFAULT_THREAD_PRIO?
Thank you for your efforts!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.