2018-11-21 3:44 PM
Just upgraded to STCubeMX v5 which appeared to successfully open a project I just started. After agreeing to the annoying "Project has been changed, do you want to save" pop-up, Atollic became non-responsive. Is this a known bug? You have coded a race condition between the timer pop-up and the main GUI thread...
PS: "Update" from previous version of STcubeMX failed (lots of downloading and thrashing, error message flashed quickly onscreen, no installation). I had to deinstall the plug-in and then install the new version after manually downloading from ST site.
PPS: Restarting Atollic, STCubeMX seems functional...
PPS: Just repeated this problem. I was working in SPI configuration when annoying question popped up, I clicked "Save", and Atollic IDE went non-responsive. There's a race condition bug between the pop-up and editing...
2018-12-07 7:31 AM
@Markus GIRDLAND - Sorry, yes its 9.1 with 5.0 plug-in, on Windows 10. I don't know the frequency; I was editing pin setup for some time (hour or two total?) and this lock-up happened twice. Clicking "No" (don't save) seems safe; only locked up when I clicked "Yes" to save. This PC is quad-core so perhaps deadlock is more likely. Sorry I can't give an exact sequence to reproduce...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.