STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM34CubeMX does not start

Posted on October 20, 2014 at 11:39I had CubeMX installed and working fine. Then I updated the application and now all I see is dialog flashing by the says ''Check files''. After that nothing happens. When I start it from a DOS box I get: java -jar ...

CubeMX 4.4.0 unexpected behavior

Posted on October 20, 2014 at 10:58Hi all, Yesterday I tried to align my project developed with CubeMX 4.3.1 to the recent 4.4.0 version.I did itmainly to overcome a SysTickInit issue with FreeRTOS configuration. Since the regenerated project compil...

DD by Associate II
  • 2396 Views
  • 3 replies
  • 0 kudos

CubeMX 4.3.1 - FreeRTOS SysTick and HardFault

Posted on September 29, 2014 at 11:38Hello,I am using the STM32F3 Discovery Board to try out CubeMX for IAR and FreeRTOS.I have encountered the following situation, where the system hangs:SysTick_Handler is never reached. The system hangs in the Har...

George.P by Associate III
  • 3988 Views
  • 6 replies
  • 0 kudos

STM32CubeMX 4.3.0 : delete user files in project folder

Posted on July 07, 2014 at 13:26Hi, Up to MX 4.2.0 it newer happends, but after upgrade MX to 4.3.0 time to time all user project  files are deleted in project folder!. STM32CubeF4  1.3.0 Windows 7 x64,  Eclipse 4.3.2 + STM32CubeMX 4.3.0 plugin. It...

gk by Associate II
  • 1009 Views
  • 1 replies
  • 0 kudos

STM32Cube, LwIP, not work TCP?

Posted on October 21, 2014 at 15:28Hello. Please help.I uses: STM32Cube 4.3.1 + STM32F407 (STM3240G_EVAL) + KeilI configures: Ethernet MII + LwIPI adds ''tcp_echoclient.?'' and ''udp_echoserver.?'' from an example (http://www.st.com/web/en/catalog/t...

use STM32F2 Cube for STM32F1

Posted on October 16, 2014 at 05:56I want to fix STM32F2Cube suitable for my device using STM32F107. My device use USB and CAN functions of MCU Certainly, I will modify HAL of STM32F2 cube First glance, I noted that USB and CAN pins of STM32F2 are s...

STM32CubeMX won't configure PA7

Posted on August 19, 2014 at 11:25Hi all,I am trying to configure a STM32F302VBTx using STM32CubeMX, and I am experiencing a strange behavior with ADC2/IN4 (PA7).Steps to reproduce: create a new projectpicks STM32F302VBTxenable ADC2 IN3 as single ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.