STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

USB CDC CubeMX bug in generated code

Posted on February 06, 2016 at 22:31 Hello, in the file usbd_cdc_if.c there is this function: uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len) { uint8_t result = USBD_OK; /* USER CODE BEGIN 7 */ USBD_CDC_SetTxBuffer(hUsbDe...

taraben by Senior
  • 1342 Views
  • 3 replies
  • 0 kudos

help in can transmission

Posted on April 13, 2016 at 18:02hi all i get for transmission data with using can protocol with stm32f429, i studied ''can primer'' article from keil.com also reading user manual of ''stm32f429'' . i configured can parametrs an all of things we ca...

mpooyesh by Associate II
  • 3058 Views
  • 7 replies
  • 0 kudos

CubeMX 4.14 ignores Keil additional targets for compiling

Posted on March 28, 2016 at 13:40I use additional targets for tweaking compiling at different stages of the project: - move in memory - set Vector table offset - compiler defines - user defines to create bin files I use stm32f437 Now when I recreate...

taraben by Senior
  • 1250 Views
  • 3 replies
  • 0 kudos

stm32cubemx & SDRAM initialization

Posted on April 20, 2016 at 18:08HiI use current stm32cubemx & cubef4 1.11i set in cubemx pins , clock & SDRAM config and generate codewhen i see sdram initialize code seems it not set auto refresh commandsthen configuration of sdram in cubemx not g...

Please fix one-year old bug!!!

Posted on April 19, 2016 at 20:03 Dear ST, please fix already one-year old bug! It is described here yet: https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM...

sincoon by Associate III
  • 2944 Views
  • 6 replies
  • 0 kudos

STM32Cube: adding user files to project in Keil

Posted on December 29, 2015 at 13:17Hi all,Hi All,I'm building a project in STM32Cube for Keil uVision 5. It's working fine. In next step I'm adding some new files in Keil, adding library path in Options for Target and when I have one more time Gene...

Two bugs in CubeMX generated code.

Posted on April 13, 2016 at 23:29For STM32Cube_FW_F4_V1.11.0:1) mxconstants.h does not have the &sharpifdef statements to guard against multiple includes.2) stm32f4xx_hal_msp.c has ''/**tttttttttt'' as the first line. It looks like there is some cra...

CubeMX Custom USB Hid Receive Data

Posted on April 05, 2016 at 16:11Hi Everyone I develop USB Hid application on STM32L0.I sent to data STM32 to Computer.But I m not receive any data from computer.Which CubeMX api I am use or how can i write my own function for receive data from usb...

STM32CubeMX 4.14.0, USART AND UART

Posted on April 03, 2016 at 13:45I generated code with CubeMX 4.14.0 for STM32F4 USART1. What I got is mainly for UART.In stm32f4xx_hal_conf.h, UART module is included, not USART&sharpdefine HAL_UART_MODULE_ENABLED//&sharpdefine HAL_USART_MODULE_ENA...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.