STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Regenerating code in CubeMX results in error

Posted on May 24, 2016 at 14:20I have a problem regarding CubeMX: the first time I generate the code, it works fine; but everytime I regenerate code and I open the project, an error occurs:cannot find entry symbol Reset_Handler; defaulting to 080000...

anio1491 by Associate II
  • 1220 Views
  • 2 replies
  • 0 kudos

STM32F072RB nucleo: CAN_handle issue

Posted on May 19, 2016 at 00:35I'm working with a STM32F072RB, a Nucleo64 series board.I'm developing CAN communication and I've some issue during the initialization of the ''CAN handle''. I use CUBE MX and stm32cubef0 libraries for the initializati...

CubeMX Feature Request - FreeRTOS alternate clock.

Posted on May 12, 2016 at 23:32In order to take full advantage of Tick-less Idle for Power-Saving I need to use an RTOS clock-source other than the SysTick.I need to alter the system clock (FreeRTOS does not accommodate this), and to do STOP1 or STO...

mattreed9 by Associate III
  • 2891 Views
  • 7 replies
  • 0 kudos

STM32CubeMX FATFS SD card re-insert

Posted on May 11, 2016 at 10:39Does anybody know how to solve the re-inserting the SD card ? I have a project generated by STM32CubeMX. I have used it for re-inserting the SD card this function: if (CD_CARD == b_cd) {   if (CD_NO_CARD == b_cd_last)...

Bug report CubeMX V 4.14.0

Posted on May 11, 2016 at 15:47Cube is corrupting the .cproject file, resulting in no symbol table for the debug elf file.Create a project with Cube, edit run, test etc.Create a 'Release' build (No-debug).Back into Cube, modify and re-generate.Back ...

mattreed9 by Associate III
  • 1108 Views
  • 1 replies
  • 0 kudos

STM32F446RE-Nucleo Board CAN Bus Exmaple

Posted on May 11, 2016 at 12:15Hello,      I am new to HAL Libraries. Can anyone please provide with an example of CAN Bus for STM32F446RE-Nucleo Board using HAL libraries. as it will help to have an idea how should we program.Thanks in advance. ...

ninad911 by Associate III
  • 3502 Views
  • 1 replies
  • 0 kudos

Bug Report STM32 CubeMX 4.14

Posted on May 06, 2016 at 05:09I use STM32CubeMX 4.14. It has little bug at MCU selector.When I checked ''ADC 16-bit'' and set the number as 1 at 'Peripheral Selection',CubeMX returns 22 items.But the 6 mcu(STM32F410xxx ) of 22 item dose not have a ...

0690X00000604uRQAQ.png
alfee0g by Associate
  • 1075 Views
  • 1 replies
  • 0 kudos

BSP functions in CubeMX

Posted on May 03, 2016 at 22:24Hi,I'm using CubeMX and System Workbench by AC6 on STM32F407-vgt6 to develop some basic projects for university purposes. First of all I'm studying Cube firmware's examples to understand how to work with the board in t...

andre-83 by Associate
  • 1878 Views
  • 3 replies
  • 0 kudos

HAL_GetTick() crash mcu

Posted on April 28, 2016 at 10:17I created a simple project using STCubeMX for my nucleo-f446ZE(STM32F446ZET6).The project should be a USB device HID but it fail to start. After messing around with the debugger, I discovered that the MCU PC register...

thom_as by Associate II
  • 2425 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.