STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX support for SD+FatFS+SPI

Posted on October 10, 2017 at 21:22 I would like to see CubeMX support for SD cards + FatFS using an SPI driver option. Both for MCUs that don't don't support SDIO and also on MCUs that have SDIO but where SPI fits the project better. FatFS is th...

Resolved! Can't get STM32F10x and CubeMX HAL I2C driver to work

Hello,i try to get a most simple I2C driver to work. So, i setup I2C1 with CubeMX and select code generation.In the resulting main.c, all i have to do is to add something like that: /* USER CODE BEGIN WHILE */ while (1) { uint8_t value = 0;   ...

SF49ers by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

STM32CubeMX config does not seem to work for systick

Hello all,I'm encountering an issue with a custom board I've made with a STM32L011D3 MCU on it.I am trying to run a very simple blink program to check the global functionalities. It looks like the code generated with STM32CubeMX does not work for the...

Loïc by Associate II
  • 1223 Views
  • 1 replies
  • 0 kudos

Problems with CubeMX v5.0.0

Hi,I was working with CubeMX v4.27.I've installed CubeMX v5.0.0, and loaded an existing project.When trying to generate code I encounter problems during download some item CubeMX requires.Please find attached screen shots.Thanks,Aviv

AFink by Associate III
  • 4143 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.