STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX error during project generation

Hello! I use CubeMX ver.5.1.0 and Linux Mint 19. When i push the button "Generate code" CubeMX creates source files and headers, but doesn't creates any project files or makefiles. Than it shows error message(screenshot in attachments). It shows this...

0690X0000089LYsQAM.png
RAkma by Associate II
  • 2333 Views
  • 4 replies
  • 0 kudos

FATFS Code Generation for STM32L (CubeMX)

I am using STM32L476VG and I want to write files to a SD card. In CubeMX I generate code for the FAT File System with the following settings:Moreover, I am using FreeRTOS with static memory allocation only:However, I have found two issues so far:Sinc...

0690X000006ByBOQA0.png 0690X000006ByBYQA0.png
OHaal by Associate II
  • 2587 Views
  • 4 replies
  • 0 kudos

USB and FreeRTOS in STM32L4

Hope someone that has implemented FreeRTOS with USB can provide advice on what specifically needs to be changed in the USB Host code to allow the USB to operate in the RTOS environment. I have USB functioning on the target board, without FreeRTOS. Wh...

CubeMX update & where to set usb/cdc & set clocks?

Discovery with stm32F407VG t.​Hi, after update I cant find place ​where I can configure usb/device/cdc like "BAUDRATE, STOP BITS"​In old version this was under "configure" usb hf. Now I can only see 12Mhz full speed.​Other issue I have is minor, Cube...

oeliks by Senior
  • 1145 Views
  • 1 replies
  • 1 kudos

STM32CubeMX v5.1.0 DOESN'T GENERATE SysTick_Handler!!!!!

Because SysTick_Handler is defined as weak, with a fallback to Default_Handler (which is a infinite while loop), this means the first time your program generates a SysTick event, your program crashes.Hopefully this post prevents others from wasting a...

TDK by Super User
  • 1884 Views
  • 3 replies
  • 1 kudos

STM32CubeMX 5.0 under Linux

Hello,I installed new STM32CubeMX 5.0.0 on my computer under Ubuntu 18.04. After start, program doesn't response. When I run it via terminal, I have some warns and error. Below I attached logs from terminal. After the last line of this log, I don't h...

Little problem from STM32CubeMX to TrueStudio

Hello,I' using Windows 7/64, True Studio 9.2, STM32CubeMX 5.1 on a Nucleo-F401RE.After code generation (GENERATE CODE) , if I try to open the project from Cube, the system answers : " Please Install TrueStudio Toolchain to open the project". I solve...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.