STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Is it possible to connect two stm32 board through usb ?

Hello,this is the first time I apply in this forum and I hope that I find the right answer to my question.So, my goal is to connect two stm32 cards (for example: STM32F4) via USB.Is it possible to do that? If yes ? how can I configure both cards with...

MBOUH by Associate
  • 2235 Views
  • 3 replies
  • 0 kudos

CubeIDE - the CubeMX part suggestion

Hi ST,this is really not a question but suggestions.When starting a project for STM32F7x board almost 1.3 GB (!) STM32Cube_FW_F7_V1.15.0 file gets downloaded. The download often breaks, it seems like download error handling and resume is not implemen...

TDJ by Lead
  • 940 Views
  • 1 replies
  • 0 kudos

Problem with acquisition of IP address of the Nucleo F746ZG

Hello everyone!I have some troubles with obtaining the correct IP address of my MCU.I am running Nucleo F746ZG and I have set up LwIP stack with CubeMX. Also DHCP is turned on. DHCP server sets up "static" IP for my MCU which is 192.168.10.88. I can ...

MZysk by Associate
  • 955 Views
  • 0 replies
  • 0 kudos

CubeMX: enables code optimizations upon code generation

I believe I am experiencing a bug in CubeMX software which is not critical but is very annoying. Every time I re-generate project code from Cube, it automatically alters .cproject file, resetting C code optimizations to -O2 level. This then leads to ...

STM32CubeMX 5.1.0 FreeRTOS code generation problem for statically generated tasks, mutexes , etc... if they were to be recreated.

Hello,During my development I came across this (sort of) bug which will require manual code modification if a specific FreeRTOS function is to be used.** Definition of the problem **FreeRTOS V9 has a feature to define the TCB of a task in compile tim...

How do I get an example created with a cubeMx?

Hello,I am looking for an example of STM32FDiscovery. So I found STM32FCube_FW_F4_V1.24.0.​STM32Cube_FW_F4_V1.24.0\Projects\STM32F4-Discovery\Applications\FatFs This example worked.​Create USB MSC + FATFS project with CubeMx. I wrote the code using t...

SWoon by Associate II
  • 921 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.