STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

After generation in the new version of CubeMx 5.2.1, the working code with tcp server is no longer detected on the network. What could it be?

After generation in the new version of CubeMx 5.2.1, the working code with tcp server is no longer detected on the network. The code is based on the tcp echo server recommended in STM32Cube_FW_F4_V1.21.0. The ethernet and lwip code and settings have ...

IHasa by Associate
  • 723 Views
  • 0 replies
  • 0 kudos

Why can't I enable all 4 SAI ports on STM32H750/STM32H743?

Hello, I am attempting to use all 4 sai ports as one large synchronous audio device.The I want SAI1A to be the master, and SAI1B, SAI2A, SAI2B, SAI3A, SAI3B, SAI4A, SAI4B to all be synchronous slaves to the SAI1A.I am able to configure them all, exce...

caleb by Associate III
  • 1993 Views
  • 4 replies
  • 0 kudos

STM32CubeMX and Keil MDK integration

Hi Guys,The latest version of STM32CubeMX allows me to use firmware packages for the F7 architecture versions 1.13.0 and 1.14.0. The latest version of the Keil STM32F7xx_DFP 2.11.0 (2018-09-05) says it uses firmware package version 1.12.0. Unfortunat...

HMcKi by Associate III
  • 1045 Views
  • 0 replies
  • 0 kudos

STM32F100RB Clock Skew In RTC and HAL_GetTick

Hello, all.I'm using the STM32F100RB , mounted on the STM32VL Discovery board.The clock confioguration, done in STM32CUBEMX is supplied at the end of the post.I wanted to use HAL_GetTick to get approximate millisecond resolution for the RTC.After som...

0690X000009YJk7QAG.jpg
ISeed by Senior
  • 2479 Views
  • 3 replies
  • 0 kudos

Resolved! Generating Code Does Not Copy Files to STM32F7xx_HAL_Driver

Attached is the IOC file I am using. When I generate the project, the STM32F7xx_HAL_Driver directory has a few folders inside of it, but none of the HAL files, including the stm327xx_hal.h file which prevents compiling from working. I have the "Copy ...

About configuring the pins.

We are using STM32F207ZG and while configuring it with the help of STM32IDE we are facing some conflicts like we have used USART1(Asynchronous mode with only Rx and Tx) . It is showing conflict if we use USART1_CTS and USART1_RTS pins as GPIO pins. T...

AR L by Associate
  • 1315 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.