STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32L476G-DISCO USART NOT WORKING?!

I'm using an stm32l476G-DISCO and i want to transmit a message using the usart, the code compiled with no error using the CubeMX but the terminal is not showing anything.i configured pin P5 as TX_USART2 and P6 as RX_USART2is it a usb driver problem? ...

OGaie by Associate III
  • 4361 Views
  • 4 replies
  • 0 kudos

CubeMX generated _sbrk() syscall does not work with freeRTOS enabled. Is there a recommended _sbrk that work well with freeRTOS? And if so, what is it and could you include it into CubeMX that is enabled only if freeRTOS is activated.

I found others have similar issue, but they are trying to work around it instead of putting in a bug report: https://community.st.com/s/question/0D50X0000AAIEWbSQP/stm32cubemx-generated-sbrk-in-syscallsc-not-working-with-freertosI was trying to do a ...

0690X000009YZHGQA4.png

Resolved! Cannot use SPI and PWM DMA together on STM32F103VET6

I'm using CubeMX for code generation.I configured my MCU (STM32F103VET6) for PWM generation on Timer 2 Channel 2 using DMA (DMA 1 channel 7), Memory to Peripherial; PWM data stored in array.All works good, if I fill data array programmatically.When ...

Vthe by Associate II
  • 1832 Views
  • 2 replies
  • 0 kudos

Timer IT fires directly after initialization

STM32F030, CubeIDE generated skeleton, TIM14 is at LL. After running MX_TIM14_Init() , TIM14_IRQHandler immediately invoked. I put a breakpoint into TIM14 IT routine, start debug, then F6 step from the beginning of main(). Please see attached video. ...

Resolved! Comp 6 and 7 not start

I have problem with comp6 and 7 I try to enable bout cannot enable comp1 -5 work without problem may be must enable clock for comp6-7

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.