STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

I am working with STM32F407VGt6-DISC1, I am facing a problem in getting LSE clock frequency out of MCO1 pin, and also other external source of clock whereas the same process for internal clock measurement through i worked fined.

Here i attached my main.c file.andWhen I run my debugger , i see that my program is stucked in error handler//////////if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}//////////And for measuring internal clock ...

VChou.1 by Associate
  • 2122 Views
  • 1 replies
  • 0 kudos

Right way to Enable/Disable/Re-enable ADC?

Hello:There is a significant amount of time between calls to the ADC peripheral and to save power I would like to shut it down. It does not seem the same as setting it up as it has issues running after.The order it initializes:MX_ADC1_Init();HAL_ADCE...

ADC DMA triggering using timer

I am using stm32f103c8t6 and performing ADC sampling of voltage input 50 Hz from the mains. I have all hardware and PCB prepared. I am achieving 60 samples/cycle using DMA mode in ADC conversion. Now I would like to know the RMS calculation algorithm...

Resolved! Generating code for SPI using DMA issue

Hi,I'm working on NUCLEO-H743ZI board, using the STM32CubeMX 5.4.0 tool.When i'm generating code for SPI using DMA - It seems that it doesn't work.I tried to generate the same code for another device (STM32F411 Discovery Board) and i sow that there...

AGutm.1 by Associate
  • 1686 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.