STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Lwip problem with Stm32Cubemx 6.1.0 and stm32H7

Hi, My project is on a Stm32H7 I'm using freeRTOS and LWIp. For testing I'm using a sample project generated by cubemx and http_netconn web server.When I generated the project with cubemx 5.6.1 it's working good.With CubeMx 6.0.1 http request are r...

VAUDI by Associate II
  • 2414 Views
  • 4 replies
  • 1 kudos

Resolved! firmware can't migrate to a new version

When I open my first project, I get a message saying that firmware must be upgraded. I clic the button 'migrate'. It works a long time. If I go to the project parameter, it is still the old firmware. And if I quit cubemx and restart it with the same ...

0693W000005C859QAC.jpg 0693W000005C8ASQA0.jpg
MJean.3 by Associate III
  • 2255 Views
  • 4 replies
  • 0 kudos

how to use algobuild in cubemx?

I tried but it didn't work. these setting is right?it makes error at TIM_AB_Config() ​Has anyone succeeded to use x-cube algobuild?​​​​

0693W000005Bl0UQAS.jpg
kdok .1 by Associate II
  • 2639 Views
  • 4 replies
  • 0 kudos

New project with CubeMX to 769I-disco

Posted on February 11, 2018 at 17:06I'm new to ARM and I brought a STM32F769I-DISCO.Creating a new project with the CubeMX all the SDIO are pre-configured as INPUTS even the ones connected to the USER-LEDs.Did someone find the same mistakes? Could i...

STM32CubeMX seems so ignore Flash TCM setup.

I am pretty sure that old versions of CubeMX (maybe years ago), when generating for TCM interface generated different code than when generating for AXI.At least in the generated STM32F765VGTx_FLASH.ld (I'm working with a F765), I had a base flash add...

raffin by Associate III
  • 1658 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F769I-DISC1 only 64Mb accessible?

Hi everyone!I'm new to the forum so please let me know if I should add more information, etc..I am using the external SDRAM (MT48LC4M32B2B5-6A, 128Mb) on the STM32F769I-DISC1 board. The SDRAM was configured with CubeMX to use all four memory banks. E...

FGeig.1 by Associate III
  • 4099 Views
  • 18 replies
  • 0 kudos

Resolved! STMCubeMX MDK-ARM project generation have a problem

Hi I am facing issue with the "generate code" to generate the boiler plate code for the nucleo-f44rehere is the software that I am running with :STMCubeMX_v6-0-1Keil ARM-MDK 5.32java version "1.8.0_271" (Java 8 I believe) , which is the recommended v...

0693W000005Bu6gQAC.jpg 0693W000005Bu7jQAC.jpg
PPoob.1 by Associate III
  • 5938 Views
  • 12 replies
  • 1 kudos

STM32CubeMX: Project generation have a problem

Hello, I am using STM32CubeMX version 4.26.1 and Keil uvision5. For a simple LED blinking example, I have made a model in Matlab/Simulink (both in version 2017b and in version 2018a). However, when I click on "build model" on Simulink, I receive an e...

0690X000006By3UQAS.png
OYava by Associate
  • 3908 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.