STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX AI 5.1.0 BUG: Cannot analyze the neural network

Hi!I have to report a bug. I cannot analyze the neural network in STM32CubeMX 1.3.0. I don't use 1.4.0 because they won't work with FreeRTOS.How to repeat this issue:Start a new Project.Select STM32 F446RE Nucleo boardUse CubeMX AI 5.1.0Download Mobi...

DMårt by Lead
  • 2797 Views
  • 2 replies
  • 0 kudos

Resolved! Requesting Fix: STM32CubeMX series 6 version (including version 6.1.0) deletes all folder present inside the main folder thus deleting user created folders like Repository

Hello @Khouloud ZEMMELI​ ,I install STM32CubeMX to folder C:\STM32CubeMX and then set REPOSITORY FOLDER TO C:\STM32CubeMX\Repository as I want to keep the STM32CubeMX and its dependencies at one place.I have reported earlier this issue either on the ...

Couldn't set ADC+DMA to work on STM32F107 with CubeMX

Hello everyone. I'm trying to setup ADC in my STM32F107, configuring it with CubeMX (ver. 5.4.0, MCU package 1.8.0), but, I fell into issue. Multiple issues, actually, but I should start with just one now, I guess.I notice odd behaviour, while I'm tr...

zedeg by Associate III
  • 2399 Views
  • 1 replies
  • 0 kudos

Queue Read from ISR and Queue Write from ISR related issue, when using file GCC\ARM_CM4\port.c and software interrupts on STM32H753BIT6

Hello @ASELSTM , @Khouloud ZEMMELI​  ,To observe the below reported issue it is mandatory that macro configASSERT_DEFINED == 1The issue is observed inside the function void vPortValidateInterruptPriority( void )which is available with FreeRTOS file G...

Resolved! Working with MCO1 pin of H7 series...

Dear experts,I am using STM32H750 vbt6 in my project .Recently I decided to use MCO1 to produce clocks for other devices attached to this chip .Also, I am using STM32cube IDE for working .It seems that setting the right parameters for MCO1 to work pr...

HTajb.1 by Associate III
  • 4417 Views
  • 4 replies
  • 0 kudos

When is cubeIDE ever going to be fixed?

I've tried multiple versions and searched the form. After generating a .IOC i cannot generate code because cubeIDE cannot handle downloading and installing new firmware on its own. Why has this issue been known about for over a year and from what i s...

CRile.1 by Associate II
  • 6385 Views
  • 11 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.