STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

RT-Thread Studio IDE v2.1.0 Release, New add 20+ ST Boards!

Hiii guys, RT-Thread Studio IDE v2.1.0 is out now. Thank you to you all who made this release possible. In this release: - 20+ New ST boards are supported. - RT-Thread Studio is now in collaboration with STM32CubeMX, where you can open CubeMX Setting...

CLi.4 by Associate II
  • 2040 Views
  • 2 replies
  • 0 kudos

STM32H7 DFSDM+ADC - bugs in CubeMX/HAL/generated code?

Using the latest CubeMX 6.2.1 and STM32H7A3 I try to accomplish, one would think, a very simple task: filter data from ADCs using DFSDM.Objective: capture N samples (conversions) on demand (e.g. button press) from several ADC channels, smooth edges w...

TDJ by Lead
  • 2401 Views
  • 1 replies
  • 1 kudos

QSPI+Flash with DMA not working properly.

Hi, I am struggling to make QSPI+Ext Flash and DMA to work for several days, but having issues.I was using BSP library for both external SDRAM (with FMC) and Flash with QSPI.However, BSP library had DMA read/write for FMC SDRAM, but not for QSPI Flas...

KMaen by Associate III
  • 2740 Views
  • 3 replies
  • 1 kudos

Hello everyone, I used a Nucleo board STM32F429ZI to develop my application. My application uses a Wiz5500 Ethernet module to communicate with another host program and performs some actions based on the received commands.

The SPI rate is at 21MBit/s and I use STM HAL.Data rate is high and I receive up to 1 message all 3ms. After I tested my application I wanted to port it to a G4 to use a cheaper microcontroller. When using the same code on the Nucleo G474RE and G431R...

0693W000008z917QAA.png 0693W000008z91HQAQ.png 0693W000008z91MQAQ.png 0693W000008z91bQAA.png
Hanni by Associate
  • 1446 Views
  • 1 replies
  • 0 kudos

STM32H723 "cannot load this MCU"

Hi there,Trying to use an STM32H723 MCU (as that's the cheapest thing right now that seems available with Ethernet, yay semiconductor shortage...)For some reason it's coming up with "STM32CubeMX cannot load this Mcu".Is there a beta/update I can down...

MHunt.1 by Associate
  • 1598 Views
  • 2 replies
  • 0 kudos

Resolved! Need help to get PWM running with NUCLEO-H743ZI2 board

Hello,I am trying to generate a PWM signal with the help of several guides from internet that ultimately contain the same thing, but it does not work, I'm doing something wrong, but I cannot see what. As a result, I only see a zero line in the displa...

STM32cubeMX - cannot unzipped

I am trying to generate code using stm32cubeMX. During code generation pop-up appreasres and shows the following error.Error downloading files:stm32cube_fw_h7_v180.zip(cannot unzipped)

0693W000008z46CQAQ.jpg
AFaya.1 by Associate III
  • 2716 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.