STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

i need cubemx 5.0.6 version .

I need cubemx 5.0.6 version for custom HID HS in STM32H743iit6.I also checked new version cubemx 6.11 but its not working. Because i am using ULPI USB3300  for high speed (HS) USB , it  require PLL clock 480MHz. But newer cubemx not supported 480MHz ...

Rajasiva by Associate II
  • 4999 Views
  • 5 replies
  • 0 kudos

Resolved! USB without VBUS

I am trying to send data with an STM32F105RB microcontroller. I have configured it using STM32CubeMX with USB_Device as CDC (Virtual COM Port) and USB_OTG_FS in Device_Only mode. I have not activated SOF or VBUS. Here is the code I am using: while (1...

luxae by Associate II
  • 2168 Views
  • 1 replies
  • 1 kudos

Resolved! Default optimization level for a project created by MXCube.

I have a project that is created by Cube for the Keil compiler.The MCU is the STM32L486VG family.The default optimization level in that project is set to -O3 but I'd like it to be -O0.I cannot see where the default value gets set. I am assuming that ...

Pevy.Andy by Associate III
  • 2624 Views
  • 4 replies
  • 0 kudos

How to choose stm32G431 BOOT mode

How to choose stm32G431 BOOT modeCan you use stm32cubemx to configure BOOT mode? If you cannot use stm32cubemx how to configure.May I ask if it is configured to boot from user flash memory.

km naxin by Associate II
  • 3808 Views
  • 4 replies
  • 1 kudos

USBX not letting me set "Hardware IP"

CubeMX: 6.11.1Im trying to implement USB dual role on STM35U5G9 When I tick "Device Controllers HS" for host and device and generate code it sends a warning I checked the Platform Settings tab and there are no options I can Change for "Hardware IP" 

PhilipC_1-1714570699012.png PhilipC_0-1714570686631.png
PhilipC by Associate III
  • 1448 Views
  • 2 replies
  • 0 kudos

Wakeup pins for STM32F030xC are missing in CubeMx

Hi everyone.I am selecting in CubeMX STM32F030xC MCU.I see on the screen case where STM32F030CCTx LQFP48 is written.Then I open Datasheet. There is Table 1. Device summary.STM32F030xC corresponds to STM32F030CC and STM32F030RC.Ok. Then I look at pino...

load2005 by Associate III
  • 1701 Views
  • 2 replies
  • 0 kudos

Resolved! FW_H7 V1.11.2 broke ADC configuration selections

Ops!!!  The latest firmware does support internal channel selection on ADC3.I verified that the previous firmware V1.11.1 gives visibility to the ADC3 internal channels for VBat, Temperature, and RBUF.  But if the firmware is migrated to V1.11.2 thos...

GreenGuy_0-1714508582404.png GreenGuy_1-1714508728898.png

Resolved! HID keyboard not working on STM32F722ZE (NUCLEO-F722ZE)

Hi guys,I'm trying to use STM32 as a host for a HID keyboard and mouse.I have 2 wireless mouses to test (Logitech M560, HP Spectre 700), Logitech T-BC21 wired trackball, some low-end keyboard. I'm connecting them via micro-USB to USB converter that w...

kaamil1984_0-1699847319586.png kaamil1984_1-1699847352678.png

Resolved! STM32F103 & SDIO - card won't respond

Posted on February 09, 2017 at 02:08I've got a custom board with a STM32F103 that connects to a micro SD card using 1 bit SDIO. I've generated some basic test code using STM32CubeMx Rev 4.19.0 and STM32CubeF1 release 1.4.0 (both the latest according...

peterm by Associate II
  • 4155 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.