STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Add WolfSSL to a LwIP example?

Using Nucleo 32H723ZG board, would like to add WolfSSL to it  Working on an SSH server app.Using the LwIP_HTTP_Server_Socket_RTOS example... watching this video:https://youtu.be/pUd2HEfBp3w?si=jiB2MysS9unIuVDr&t=1727It appears that my problem is this...

st3ph3n by Associate II
  • 2610 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H730ZB - SDRAM BANK1 wrong address

Hi, I create a new project with STM32CubeIde 1.15.1 (but same with 1.10.1)I add SDRAM 1 - BANK 1When I debug this project, after HAL_SDRAM_Init function in MX_FMC_Init(), I can wath the memory in MEMORY BROWSER at address 0x60000000.But on reference ...

COSEBE_0-1718065782758.png COSEBE_2-1718066108988.png COSEBE_3-1718066173657.png
COSEBE by Senior
  • 7329 Views
  • 12 replies
  • 1 kudos

USB (Mass Storage Class) Not detected in STM32F405

Dear All,        In my project, I am using STM32F405RG MCU for file read/wirte operations using FATFS.I declare the physicaldrive as USB DEVICE (Mass storage Class) ,while I am generating a  code  for USB DEVICE(Mass Storage Class) its only works for...

Kavinraj by Associate III
  • 1925 Views
  • 2 replies
  • 0 kudos

Stm32h7 Ethernet

Hi, I am frequently getting tired while working with the STM32H743ZIT6 144-pin Nucleo board / STM32H743IIT6 controller board and an externally connected Ethernet module using a communication protocol. Despite trying many different ways, it is still n...

Using STM32CubeMX 6.3.0 with a dual core STM32H755 micro there is no obvious way to set GPIO context so the same CubeMX pin is defined in both cores

Using STM32CubeMX 6.3.0 with a dual core STM32H755 micro I have a dip switch I wish to be able to read from both cores. Some peripherals (like TIM1 for example) have check boxes for runtime contexts that let you check M7 and M4 to access the peripher...

GHolc.1 by Associate III
  • 2168 Views
  • 2 replies
  • 1 kudos

Don't enable interrupts

I would like to know if there is a way to NOT enable interrupts during the initialization of the EXTI. See below for snippet /* EXTI interrupt init*/ HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(EXTI0_IRQn);   HAL_NVIC_SetPriorit...

Clock Configuration Report

The STM32CubeMX has a Clock Configuration page that can be captured in the "Generate Reports"I like to Print this page to configure clock timings and divide counters.  The problem is that many of the values are very light, the ones that you can't cha...

DWise.1 by Associate II
  • 1507 Views
  • 1 replies
  • 1 kudos

CubeMX Freeze When Generating Code

Every time I try to generate code using the latest version of CubeMX, the software freezes and remains unresponsive for hours. I have tried using previous versions, but the problem persists. How can I resolve this issue?Screenshot is attached below.P...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.