2024-06-11 7:37 PM
Using Nucleo 32H723ZG board, would like to add WolfSSL to it Working on an SSH server app.
Using the LwIP_HTTP_Server_Socket_RTOS example... watching this video:
https://youtu.be/pUd2HEfBp3w?si=jiB2MysS9unIuVDr&t=1727
It appears that my problem is this example does not generate an ioc file so that the pack I downloaded and put into CubeMX will not be applicable. Is this right? Will I just have to construct the example project and import it by hand?
2024-06-18 3:53 AM
2024-06-19 6:41 PM
So, I am to imply that creating a new MX project is the only way to do this? I have a working 32H723ZG example, I would like to add WolfSSL to it. I also have a working MX example, the WolfSSL example in the video. Is there no way to combine files from one into the other? Must I lose the working example to get where I need to go? Is there no way to take WolfSSL and add it to the LwIP example? I have downloaded the package, is there not a way to add it without requiring an ioc file or MX? Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.