STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX not linking files at all

Hello there :) I create a project with TouchGFX 4.24.1, then import it to CubeIDE 1.16.1, which are both the current versions. Once i open the .ioc file, it says the file need to either be migrated to 6.12.1 or I can use the file as is, which seems t...

FabianEbs by Associate III
  • 2604 Views
  • 4 replies
  • 0 kudos

Resolved! Hi there, I have to create the BSP for a product we are actually developing, based on a STM32U575RIT6Q. As FreeRTOS is not currently supported in CubeMX for this microcontroller, could you tell me which solution is the best to add FreeRTOS ?

According to my searches on the internet, I found at least 3 solutions to add FreeRTOS on top of the code generated with stm32cubeMX for STM32U5 ...1 - Get FreeRTOS from freertos.org or its GIT2 - Get FreeRTOS from the demo available on the B-U585-IO...

PToch.1 by Associate
  • 2171 Views
  • 2 replies
  • 0 kudos

Resolved! List of compatiable MCU hangs at 52%

Hello,My original project was created for STM32F030c8t6 and I want to get the list of compatible  MCU, so that I can migrate my project to STM32f103C8T6. I opened the cubeMX table from CubeIDE. While I clicked the list of compatible MCU, the programs...

Techn by Senior III
  • 2330 Views
  • 3 replies
  • 0 kudos

Resolved! Tasks created by CubeMX vs created by code

Is there any difference if I create two freertos tasks by hand in my code or if I do it using the cubemx interface?Things like preventive checks, checks that the stacks do not overlap or are too big compared to the available memory?

Resolved! Usart 3 not a available on NUCLEO H755ZIQ in CubeMx

Good morning , I have a problem on stm32: USART3 is impossible to put  into available:   the schematics of my nucleo 144 tell me however to use usart 3:    I wanted to do it manually by turning directly the pins of PD9 and PD10 into tx nd rx but it...

Jad_0-1727964328756.png IMG_9603.jpeg
Jad by Senior
  • 1829 Views
  • 2 replies
  • 2 kudos

Feature Request: Nucleo Pin Overlay

I am using a STM32 part on a Nucleo dev board. When I am looking and the main page in CubeMX I get an overview of the processor and its pins but I do not have a handy mapping to know which Nucleo pins are connected to which processors pins.Could we h...

a_user by Associate III
  • 2857 Views
  • 5 replies
  • 8 kudos

Resolved! Where is ST-LINK_gdbserver?

ST-LINK_gdbserver has been a very important part of my Arduino development with ST micros. I've used it extensively with the STM32L071 and am wanting to use it with the STMU073. But I need to upgrade it for the newer micro. So I've upgraded my CubeMX...

doctek by Associate II
  • 7708 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.